(0)| 11/21/2024 2:41 AM | |
|
Posts: 7 Rating:
|
Hi , im using iot2050 advance fs9 and im facing with this problem that after installation is complete, when i try to change the serial mode from default to RS485 , it doesn't take effect, and after reboot again with mel-setup command i find that as default. Also ive tested different setup time and hold time which i dont know if it could be the reason or not. Would you please help? I should say that i could do it one time but after another fresh installation from service stick , i could not change it anymore. ------------------------------------------------------------------------------------------ |
Last edited by: Hans Wilhelm at: 11/21/2024 02:42:44Last edited by: Moderator_Lan at: 11/21/2024 07:22:14New subject after splitting |
|
| 11/21/2024 6:09 AM | |
|
Joined: 12/18/2014 Last visit: 1/13/2026 Posts: 36439 Rating:
|
Please don't post twice for the same problem. You also made an own topic: Change mode of external serial |
Follow us on