(0)| 4/19/2024 2:03 AM | |
|
Joined: 11/21/2023 Last visit: 4/19/2024 Posts: 2 Rating:
|
Hi, We recently had multiple sites with IoT2050s fail to reboot after a remote reboot command was issued. I've attached the log from one of the sites noting the failed reboot occurred on 16 April, from the log does anyone have any idea why the IoT2050 failed to reboot. On the 18 April a power cycle was able to successfully boot the device. Cheers David Attachmentfailed_reboot.txt (550 Downloads) |
| 4/21/2024 2:26 PM | |
|
Joined: 4/28/2015 Last visit: 1/7/2026 Posts: 578 Rating:
|
Might be https://github.com/siemens/meta-iot2050/issues/440 as well. That is only fully visible via the UART debug interface. |
| 5/16/2024 3:28 PM | |
|
Joined: 6/29/2018 Last visit: 11/20/2024 Posts: 3 Rating:
|
We face the same issue.. I have seen a hardware watchdog is available in iot2050 as posted here. Did someone use that feature to solve the problem of reboot ? Best Regards. |
| 11/27/2024 7:46 AM | |
|
Joined: 3/12/2024 Last visit: 1/9/2026 Posts: 230 Rating:
|
Hello, the firmware version V1.4.3 with the workaround for this issue was published today on our Downloads Page at Industry Online Support. Further information can be found in our new forum entry "How To Firmware Update V1.4.3". Thanks |
Follow us on