(0)| 11/19/2024 12:27 PM | |
|
Joined: 5/6/2022 Last visit: 1/15/2026 Posts: 589 Rating:
|
Hi rol_dan, There is no difference in the 'Camera View' object between the 9" or smaller Comfort Panels and the 12" or larger Comfort Panels. The 'Camera View' object is available for all Comfort Panels and KTP Mobile Panels (as of device version V13) and provides consistent functionality across all display sizes (4" to 22"). The 'Camera View' object can be configured in various screens such as a screen, template, slide-in screen, or pop-up screen, and it supports network cameras that use streaming protocols like RTP/RTSP and codecs such as MJPEG, H .264, and MPEG4 (SIMATIC STEP 7 Basic/Professional V18 and SIMATIC WinCC V18: # Camera view). Additionally, there is also this application example where you can find more information: "Monitoring with Network Cameras and SIMATIC HMI Comfort Panels" This is all the information I can share with you, I hope it can be helpful. Best regards! |
|
If this Information really helps, you could use the Rate function |
|
Follow us on