(0)| 12/10/2024 12:04 PM | |
|
Joined: 3/14/2008 Last visit: 1/15/2026 Posts: 2233 Rating:
|
Hi, By default the names: Forward/Reverse and Stop are displayed. If you want to change this, you must fill in the "Text 1" attribute in the block properties of the MotRevL. By default it's empty, so the default text is taken over that is configured in the faceplate. See attached screen. |
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on