12/11/2024 11:20 AM | |
Joined: 5/27/2023 Last visit: 7/14/2025 Posts: 20 Rating:
|
Hello everybody, I have a problem with a system consisting of a S7-1511C PLC and 12 Sinamcs G120C Drives which automatically switches the PLC into STOP Mode, turns on the Error status and it remains as that, without the abillity to swtich on. I can download the commisioning from Tia Portal to each individual drive, modify its parameters and control them in Control Panel. I can ping each individual drive and the Profinet physical connections are ok, I checked each one of them with a network tester and the lapout corresponds with the network configured in Topology view. The IP's and the Device names in the project corresponds with the ones on site. I'll attach the diagnostic buffer (ignore that there are 3 devices that aren't detected, they hadn't arrived yet) and also in the first comment I'll attach a document with the configuration with some pictures for illsutration. I noticed that the same three errors persists on all the drives: on Port 1, Port 2 and ModuleAccessPoint. I hope you can help me solve this situation. Thank you for your help and for your time! Best regards, Claudiu AttachmentDiagnostics 5.txt (117 Downloads) |
Last edited by: Claudiu Muresan at: 12/11/2024 11:23:50 |
|
12/11/2024 11:24 AM | |
Joined: 5/27/2023 Last visit: 7/14/2025 Posts: 20 Rating:
|
The document with further information. Thank you! AttachmentCommunication Errors.docx (124 Downloads) |
Last edited by: Claudiu Muresan at: 12/11/2024 11:25:09 |
|
Follow us on