12/12/2024 4:48 AM | |
Joined: 6/3/2024 Last visit: 4/16/2025 Posts: 1 Rating:
|
Has anybody solved this issue. i am also facing this same kind of issue. Earlier, There was no DC link showing and in r26 dc link voltage showing 32.7V and P210 Drive unit line supply voltage is 600V. I change the drive and now the new drive give alarm F30021 ground fault, F30005 power unit overload , F7802 .....,, i checked the motor there is no ground fault , motor resistance is ok ....Please suggest what to do.. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 12/12/2024 07:46:05New subject after splitting |
|
Follow us on