12/30/2024 9:26 AM | |
Joined: 8/3/2009 Last visit: 9/4/2025 Posts: 16325 Rating:
|
Hello wondem WinCC Is only compatible and released with the SQL Server Version that is this WinCC Version delivered with (on the same Computer) So in the compatibility Tool https://support.industry.siemens.com/cs/de/en/view/64847781 only 2016 (64-Bit) SP35) and 2016 (64-Bit) SP2 is released with WInCC V7.5 SP2 (depends on the Update you use in WInCC) Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on