(0)| 5/31/2024 1:12 PM | |
|
Joined: 4/14/2014 Last visit: 9/15/2025 Posts: 1 Rating:
|
We have the same issue, when trying to browse the LOGO web server, only responds with 192.168.0.3/Multilingual_readMe_OSS.html - Siemens Third Party Disclosure Agreement. LOGO Hardware: 6ED1052-1MD08-0BA2 LOGO! 12/24 RCE with firmware 1.84.02 LOGO IP Address: 192.168.0.3 (LAN - Only LOGO to PC) PC Software: LOGO!Soft Comfort v8.4 and Microsoft Edge Version 125.0.2535.67 PC IP Address: 192.168.0.55 (LAN - Only LOGO to PC) LOGO programmed and running fine. Clock updated. LOGO has Access Control > Web Server Access enabled (HTTP) LOGO has Access Control > Web User enabled Tried - LOGO!Soft Comfort > Tools > Transfer > Certificate Settings - Root, Device, etc. certificates saved and imported into Microsoft Edge. Tried - Software and Hardware restarted multiple times. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/03/2024 07:10:28New subject after splitting |
|
| 5/31/2024 1:24 PM | |
|
Joined: 12/18/2014 Last visit: 1/16/2026 Posts: 36463 Rating:
|
Start a Support Request. |
| 1/9/2025 10:41 AM | |
|
Joined: 4/19/2024 Last visit: 1/16/2026 Posts: 31 Rating:
|
Same here, can't access to the web server and the same message |
Follow us on