(1)| 12/27/2024 8:54 AM | |
|
Joined: 6/22/2023 Last visit: 1/7/2026 Posts: 13 Rating:
|
Hello Geniuses, I would like to make a 5 way divider control and use quality components and I chosen Siemens LOGO. I would like to use a potentiometer to choose where the product goes and use a gear motor to rotate the divider. My problem is to make the rotation counterclockwise,reasonably. Is it possible to use the Analog Comparator to reverse the direction of rotation??Or do I just have to run from minimum to maximum and back?? I'm a newbie with PLC so I didn't come up with a solution... .so I Greatly Appreciate the answer. AttachmentDivider.zip (289 Downloads) |
Last edited by: Moderator_Lan at: 12/27/2024 10:18:42Text formatting optimized |
|
| 1/8/2025 6:34 AM | |
|
Joined: 6/22/2023 Last visit: 1/7/2026 Posts: 13 Rating:
|
However, I want to try the potentiometer and I must fix the program so that the direction of rotation dont change when the limit is not coming from the sensor. Or should I just give up??? AttachmentDivider AnalogMux unfinished.zip (286 Downloads) |
| 1/8/2025 3:55 PM | |
|
Joined: 6/11/2019 Last visit: 1/14/2026 Posts: 2721 Rating:
|
It's actually not that difficult. Just use several muxers I think it's easier to modify your program than to explain everything in text. Take a closer look at it. If you have any questions, just ask in the forum. "I must fix the program so that the direction of rotation I'm sorry, I don't understand that statement.You have to be more specific. Regards Ella_68 AttachmentDivider AnalogMux unfinished mod 01.zip (294 Downloads) |
| 1/10/2025 9:59 PM | |
|
Joined: 6/11/2019 Last visit: 1/14/2026 Posts: 2721 Rating:
|
Glad I could help and have fun continuing... Greetings Ella_68 |
Follow us on