1/23/2025 1:10 PM | |
Joined: 10/27/2021 Last visit: 3/11/2025 Posts: 12 Rating:
|
Hi. |
Last edited by: Moderator_Lan at: 01/23/2025 13:47:42Link optimized / Image embedded |
|
1/27/2025 8:43 AM | |
Joined: 10/27/2021 Last visit: 3/11/2025 Posts: 12 Rating:
|
can't get tsend or put/get to work... how can it be so hard to share variable over diffrent plc in the same network? |
1/28/2025 5:38 AM | |
Joined: 10/7/2005 Last visit: 9/2/2025 Posts: 3049 Rating:
|
The screendump is hard to read but it seems you configured an S7 connection and then use (try to) use AG_SEND/AG_RECV. This will not work and you need to either change you connection to ISO-on-TCP (or TCP or UDP or ISO) as per example that you followed OR use BSEND/BRCV if you want to stick with an S7 connection. For reference and anything you ever (or never) wanted to know about communication within the Siemens PLC world, grab a copy of the CPU-CPU communication with Simatic Controllers |
Cheers |
|
Follow us on