(0)| 5/7/2021 8:10 AM | |
|
Posts: 6 Rating:
|
Hi I work on a car lift that I have some challenges with. Overview: When I6 + 7 is high, the lift is at the bottom. Q1: Hydraulic pump (lifting) I have made a counter function which starts the warning sound when it is at a certain height, 150mm. What I need help with: AttachmentLDI Prog.zip (1230 Downloads) |
Last edited by: AMR-AC-HYDRAULIC at: 05/07/2021 08:26:15Last edited by: AMR-AC at: 05/07/2021 09:35:41 |
|
| 5/7/2021 8:13 AM | |
|
Joined: 6/19/2019 Last visit: 10/24/2025 Posts: 743 Rating:
|
Hello, First add your program to help you. |
| 5/7/2021 8:27 AM | |
|
Posts: 6 Rating:
|
Now added :-) |
| 5/7/2021 9:10 AM | |
|
Joined: 6/19/2019 Last visit: 10/24/2025 Posts: 743 Rating:
|
Please also add .zip format program |
| 5/7/2021 9:35 AM | |
|
Posts: 6 Rating:
|
Done :-) |
| 5/8/2021 7:35 PM | |
|
Joined: 4/14/2013 Last visit: 8/6/2025 Posts: 33 Rating:
|
Hello. The best... E: |
Last edited by: erku at: 05/08/2021 19:48:18Last edited by: erku at: 05/08/2021 19:56:26 |
|
| 5/10/2021 7:09 AM | |
|
Posts: 6 Rating:
|
Hello! In Europe we don't have a requirement of a mechanical locking. Our standard says, that we should be able to handle one hydraulic leak. This lift is a two pillar underground with one cylinder in each pillar, so one cylinder and the mechanical structure are able to carry the entire load, with a maximal drop of 100mm. The standard says, that our main switch can replace a EMG switch. And then to your question. The lift should stop at a specific height (danger of squeeze). And then it should be allowed to lower entirely. |
Last edited by: AMR-AC at: 05/10/2021 07:22:39 |
|
| 6/3/2021 9:37 AM | |
|
Posts: 6 Rating:
|
Anyone who can help me? I work on a car lift that I have some challenges with. Overview: Q1: Hydraulic pump (lifting) I have made a counter function which starts the warning sound when it is at a certain height, 125mm. What I need help with: Thanks :-) AttachmentLIFT.zip (1263 Downloads) |
| 11/3/2024 4:43 PM | |
|
Joined: 11/3/2024 Last visit: 6/17/2025 Posts: 1 Rating:
|
If the car lift's safety stop activates when going down, it could indicate an issue with the safety sensors or hydraulic system. Check for obstructions or misalignments in the lift mechanism. Regular maintenance and inspection can help ensure safe and smooth operation.. |
Last edited by: Lisasmith at: 11/03/2024 16:44:04 |
|
| 1/31/2025 10:59 AM | |
|
Joined: 1/31/2025 Last visit: 1/31/2025 Posts: 1 Rating:
|
If the car lift's safety stop engages while lowering, it may signal a problem with the safety sensors or hydraulic system. Inspect for any obstructions or misalignments in the lift mechanism. Performing regular maintenance and inspections can help maintain safe and efficient operation.. |
Follow us on