(0)| 2/1/2025 6:17 PM | |
|
Joined: 1/12/2011 Last visit: 11/19/2025 Posts: 65 Rating:
|
Hello, I have a inp outp area size problem with a Keyence camera iv4, it takes up so much input space that a 1212c has a problem with only 1024 inputs. Only a few inputs bytes of the camera are used, rest is not used. I try to remove not used outputs bytes from camera slots so that the inputs are not exceeded but I get an error. What to do? Thanks. Moose ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 02/03/2025 08:58:13New subject after splitting |
|
| 2/3/2025 8:59 AM | |
|
Joined: 7/30/2024 Last visit: 1/14/2026 Posts: 1190 Rating:
|
Topic closed, because the question has been published twice. You can find the active topic here: Keyence IV4 Profinet connection
Kind regards, Moderator_Lan |
Follow us on