(0)| 2/11/2025 7:25 AM | |
|
Joined: 2/11/2025 Last visit: 12/17/2025 Posts: 9 Rating:
|
Dear Everyone, I am facing one issue occurring every week. The system is with S71200 1215, where this error says that, “Error: IO device failure - Connection abort by IO device Potential inhibit/break reason for next startup: - Unacceptable configuration difference (wrong or missing component)”. With an event id:16# 02:39CB The system contains four Schmersal SFB-PN-IRT -8M12-IOP RIO modules and Eight Schmersal BDF200-FB-NHK-LM-LM-LT-G24-2875 PB modules. In some moment one of 4 Schmersal SFB-PN-IRT -8M12-IOP RIO modules going in error state and in next 20 seconds all of them have same error: IO device failure - RPC application timeout. The problem is that we cannot work with the machine until we solve the communication with the module. That's why we have to stop/start the PLC every time so that the network and communication with the module is stable. For the troubleshooting even we have checked communication cables, power cables bur still remaining with the same issue. Hope you can give me some hint! Thank you in advance! ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 02/11/2025 09:02:28New subject after splitting |
|
| 2/11/2025 9:03 AM | |
|
Joined: 7/30/2024 Last visit: 1/16/2026 Posts: 1192 Rating:
|
Topic closed, because the question was posted twice. The active topic can be found here: 1200: Connection abort by IO device Kind regards, Moderator_Lan |
Follow us on