(0)| 2/18/2025 10:00 AM | |
|
Joined: 5/2/2023 Last visit: 11/18/2025 Posts: 4 Rating:
|
We have using LOGO without display LOGO V8.3 (6ED1052-2MD08-0BA1) PLC with FW Version 1.83.02 with TDE display (6ED1055-4MHO8-0BA1) of FW Version in TDEdisplay1.83.01. In this we have worked on Function Block. for message text switching we have used M27 for showing the message difference still now in V8.3 all are working good and acknowledging the message without any error on Both M27 in OFF or ON state. But, Now the new version is LOGO V8.4 (6ED1052-2MD08-0BA2) PLC with FW Version 1.84.02 is we can’t acknowledge the alarms in TDE display with the FW Version in TDE display1.83.01. When the M27 is in ON state. We were able to acknowledging all messages in M27 is in OFF state but we can’t acknowledge in M27 in ON state. As we checked the PLC (6ED1052-2MD08-0BA2) and TDE display (6ED1055-4MHO8-0BA1), in simulation all functions acknowledging without any error. And once download in PLC and TDE the above mentioned error occurs. We have Enabled all the BM setting in both TDE and PLC.
Input 1 used for M27 bit enable and disable. Input 2 used for Message Enabled. AttachmentM27_Testing.zip (220 Downloads) |
| 2/19/2025 9:58 AM | |
|
Joined: 5/2/2023 Last visit: 11/18/2025 Posts: 4 Rating:
|
Issue not solved: LOGO Without display can't acknowledge message in M27 in ON state Hi,
And Can we use same languages in Both character set in M27. Because still now we have worked like that which mean same languages in Both character set using M27 and works properly. Once LOGO V8.4 (6ED1052-2MD08-0BA2) PLC with FW Version 1.84.02 we are facing the acknowledge issues that can't able acknowledge the Message While M27 bit is in ON state. The below attached video In manual mode we acknowledge the message but in auto mode we can't able acknowledge the message. This is issue we were facing in TDE. AttachmentM27 issue.avi (208 Downloads) |
| 2/20/2025 8:25 AM | |
|
Joined: 11/3/2008 Last visit: 10/29/2025 Posts: 74 Rating:
|
Your screen shot shows you try to update to 1.84.02 (Q3 issue). But you need the update to V1.84.03, link: https://support.industry.siemens.com/cs/ww/en/view/109975995 |
Last edited by: Moderator_Lan at: 02/20/2025 08:29:37link optimized |
|
Follow us on