(0)| 2/14/2025 8:45 AM | |
|
Joined: 12/18/2014 Last visit: 1/12/2026 Posts: 36436 Rating:
|
Sales Release and Download for Firmware 3.6.17 for CP 1243-7, CP 1243-1, CP 1243-8Firmware version 3.6 for the following S7-1200 communication modules is available for download:
The firmware contains general product quality improvements and is used to upgrade devices of the above-mentioned products that are already in use. In particular, the firmware contains the following changes: Feature Enhancements: DNP3 - Point-to-Point Connection to Third-Party Devices
Optimized Event Buffer Clearing
DNP3 - Negative Acknowledgment for Time Synchronization Requests from Unauthorized Partners
IEC 60870-5 - Support for Originator Address
IEC 60870-5 - Support for COT11/12
IEC 60870-5 - Support for Multiple TCP Ports
Extended Time Tab in Online Diagnostics
Time Stamp Validity in NTP with TeleControl Applications
Bugfixes:
Security fixes:
To utilize the new "Functional extensions," customers are required to configure their modules to operate on offline version V3.6 or later. For CP1200 modules, the requisite TIA version for offline V3.6 compatibility is TIA V20. |
This contribution was helpful to
|
|
| 3/7/2025 3:47 AM | |
|
Joined: 12/18/2014 Last visit: 1/12/2026 Posts: 36436 Rating:
|
Update to Notification 109982797 – FW Version 3.6.18 for S7-1200 CPsDESCRIPTION: Firmware version 3.6.18 for the following S7-1200 communication modules is available for download:
The firmware is addressing a time synchronization issue within firmware version 3.6.17, released with the following product note: 109982797. Firmware version 3.6.17 is being recalled and immediately replaced with firmware version 3.6.18. The product note 109982797 has been updated accordingly. In case, you downloaded and installed firmware version 3.6.17, we strongly recommend upgrading to version 3.6.18. A description of how to perform the upgrade can be found in the mentioned product note. |
This contribution was helpful to
|
|
Follow us on