(0)| 3/29/2025 7:47 AM | |
|
Joined: 6/11/2019 Last visit: 1/6/2026 Posts: 2717 Rating:
|
Hello AutoGen, As already described, you can't query the Logo clock time directly in the program. There are two indirect options: One is to build an auxiliary clock that synchronizes with the Logo clock every hour. However, this has the disadvantage that after a failure or program restart, an incorrect time in the minute range is displayed until the next full hour. Or you can get the time from a second Logo. I've already described this procedure in the German section of the forum. Regards, Ella_68 (translated with Google) |
Follow us on