(0)| 12/7/2018 1:31 PM | ||||
|
Posts: 11 Rating:
|
I've done everything according to the manual(as you wrote above) and as I said, Webserver works fine so for me Logo comfort should work as well. I also installed the Logo App and there is also everything fine! I can connect to the controller with no issues. I got my Logo comfort on a CD so it is full and legal. I tried on different PC with no luck |
|||
This contribution was helpful to
|
||||
| 12/7/2018 6:51 PM | |
|
Joined: 12/18/2014 Last visit: 1/17/2026 Posts: 36469 Rating:
|
Please write us the type of the TP link router. |
| 12/8/2018 10:12 AM | |
|
Posts: 11 Rating:
|
tp-link TL-WR841N ver 13 300Mbps Wireless N Router |
| 1/24/2019 3:02 PM | |
|
Joined: 7/28/2007 Last visit: 11/19/2025 Posts: 29 Rating:
|
I suggest you to test port 102 or 103. For me was OK on Logo7. |
| 4/21/2019 12:38 AM | |
|
Posts: 1 Rating:
|
Hello Finally, I can connect with DNS, I can help yo |
Follow us on