(0)| 4/17/2025 2:44 PM | |
|
Joined: 10/17/2018 Last visit: 1/19/2026 Posts: 62 Rating:
|
Greetings. I've attached the input and output configuration. To continue with the project, please confirm if the input and output configuration meets your needs. AttachmentInterlocking Fan.zip (340 Downloads) |
| 4/17/2025 4:52 PM | |
|
Joined: 6/11/2019 Last visit: 1/18/2026 Posts: 2729 Rating:
|
Hello AutoGen, Even if I were only working with exhaust fans, here's my first suggestion. The output setup looks quite slow in the simulation. However, the Logo itself works much faster, so I assume this has some effect on the contactors. Otherwise, the outputs would have to be synchronized, which would require an additional 30 blocks. Best regards Ella_68 AttachmentLuefter 1-5.zip (329 Downloads) |
This contribution was helpful to
|
|
| 4/20/2025 8:30 PM | |
|
Joined: 10/17/2018 Last visit: 1/19/2026 Posts: 62 Rating:
|
Greetings. I hope the video showing your request at this link can help you in some way. AttachmentInterlocking Fan.zip (325 Downloads) |
Last edited by: Moderator_Lan at: 04/22/2025 06:06:47Video embedded. |
|
Follow us on