(0)| 4/25/2025 8:38 PM | |
|
Joined: 3/14/2025 Last visit: 10/8/2025 Posts: 6 Rating:
|
Hello everyone, I hope you're all well. I have a question regarding the CLOSE PICTURE event. I have some I/Os that have scripts associated with them (output value - change), and I need them to continue running even if the operator changes the PICTURE. For example, when the PLC changes a value tag, this value reaches an I/O FIELD, and this change activates the script, which basically sends other values to other tags. This works correctly until I change screens. The script doesn't run if the screen it's on isn't open. Is there any way to keep this running even if the screen changes? ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 04/28/2025 08:18:32New subject after splitting |
|
Follow us on