(0)| 4/24/2025 9:32 AM | |
|
Joined: 1/21/2013 Last visit: 1/15/2026 Posts: 4402 Rating:
|
Hi Mattias, It is not possible to access the available languages directly within the runtime. However, it would be possible to execute a script at the start of the runtime that switches the language with SysFct.ToggleLanguage() and reads the current language with HMIRuntime.Language. This would have to be repeated until a recognized language is found. However, the user could notice the language switch without any additional steps. An alternative approach would be to modify the project using TIA Portal Openness, but to be honest, I don't have enough experience with this topic to be sure that the functionality is already supported. Kind regards |
Follow us on