(0)| 5/1/2025 6:12 PM | |
|
Joined: 7/11/2024 Last visit: 12/26/2025 Posts: 200 Rating:
|
Hello aamirawan91 As a general rule, when you replace a CPU with its compatible successor, the STEP 7 project does not need to be changed. Also, note that successor that you have proposed for the second CPU is 6ES7515-2AM02-0AB0, which is also phased out. The successor of this one is 6ES7515-2AN03-0AB0 but, as there are two jumps between successor products, you proably won't be able to perform a plug and play replacement. I think you'll find useful this FAQ: How do you find the right successor product if the existing product has already been discontinued? Good luck! |
Last edited by: JimHalpert at: 05/01/2025 18:13:42If this post has been useful, don't forget to rate it!😊 |
|
Follow us on