5/13/2025 12:39 PM | |
Joined: 1/21/2013 Last visit: 9/10/2025 Posts: 4101 Rating:
|
Hi mdarende, No, not with WinCC Unified's internal scripting. The JavaScripts you create in WinCC Unified are server-based and cannot access the browser. However, it should be possible with a custom web control (CWC). The Web-Toolbox_CWC includes a similar feature, but unfortunately, it is not exactly the same. Kind regards |
This contribution was helpful to
1 thankful Users |
5/14/2025 10:33 AM | |
Joined: 1/21/2013 Last visit: 9/10/2025 Posts: 4101 Rating:
|
Hi mdarende, Breaking news! You can now use the EnterFullScreen and LeaveFullScreen functions to control kiosk mode in WinCC Unified PC RT V20 Update 2 and WinCC Unified ES V20 Update 3. Kind regards |
This contribution was helpful to
3 thankful Users |
5/18/2025 9:16 AM | |
Joined: 1/21/2013 Last visit: 9/10/2025 Posts: 4101 Rating:
|
Hi mdarende, The EnterFullScreen and LeaveFullScreen functions are only available in JavaScript. Kind regards |
Follow us on