6/2/2025 7:24 AM | |
Joined: 6/2/2025 Last visit: 8/15/2025 Posts: 5 Rating:
|
Are there any HSP files for 6ES7 338-4BC00-0AB0 |
6/2/2025 7:52 AM | |
Joined: 1/21/2013 Last visit: 8/29/2025 Posts: 4087 Rating:
|
Hi, Unfortunately, this module is not included in TIA Portal because it was discontinued on November 1, 2007. It cannot be integrated using a Hardware Support Package (HSP). Therefore, you will not be able to migrate the project, including the hardware, unless you first modify the hardware configuration using SIMATIC Manager. For more details please refer to What are the requirements for migrating a STEP 7 V5.x project to STEP 7 Professional (TIA Portal)?. Kind regards |
This contribution was helpful to
1 thankful Users |
6/2/2025 10:26 AM | |
Joined: 1/21/2013 Last visit: 8/29/2025 Posts: 4087 Rating:
|
Hi, In general, changing to firmware version V2.6 should not have an impact. Kind regards |
Follow us on