9/13/2023 2:24 PM | |
Joined: 10/25/2022 Last visit: 8/12/2025 Posts: 1 Rating:
|
Hello, Try to lunch the app "WinCCViewerRT" with "Run as administrator" Regards |
7/4/2024 5:41 PM | |
Joined: 12/17/2011 Last visit: 6/17/2025 Posts: 3 Rating:
|
Hello. |
5/8/2025 8:59 AM | |
Joined: 4/14/2025 Last visit: 6/26/2025 Posts: 2 Rating:
|
Hello everyone, I've tried connecting with other virtual machines with WinCC 7.5 installed and they have no problem connecting right away with the server, so it's not a licensing issue, it's specific of this web client. Connection to the server from the virtual machine through cmd ping command is working too. I should mention that the virtual machine used to have an old version of WinCC incompatible with Web Navigator Client, so in order to install this I had to uninstall WinCC, perhaps I over did it and uninstalled an important file, I'm not sure if that could pose problems with Web Navigator. Furthermore the machine's Simatic Shell Explorer is now deactivated, and the folder's settings look like this now (see attachment), so I wasn't able to follow the solutions proposed in this thread regarding it. AttachmentSimatic shell settings.pdf (223 Downloads) |
Follow us on