(0)| 7/3/2025 9:02 AM | |
|
Joined: 3/17/2025 Last visit: 10/30/2025 Posts: 1 Rating:
|
Hello,
But then result is that “m_trans_2” - is in state TRUE. I wasn't able to find anything what can explain me this behavior of GRAPH sequence. CPU 1517TF-3 PN/DP Attachmentpictures.zip (93 Downloads) |
| 7/3/2025 10:06 AM | |
|
Joined: 1/21/2013 Last visit: 1/11/2026 Posts: 4387 Rating:
|
Hi, It's been a while since I've dealt with this topic. However, as far as I can recall, this behavior is influenced by the block interface parameter set. When using the maximum parameter set, the T_NO parameter is added to show the valid transitions. If there are multiple valid transitions, the one with the highest number is shown by default and used. However, I think this behavior also depends on the mode used (manual, automatic, or semi-automatic). Kind regards |
Follow us on