(1)| 7/4/2025 12:41 PM | |
|
Joined: 12/18/2014 Last visit: 1/2/2026 Posts: 36394 Rating:
|
Please write the complete order number. Ends the order number with 0BA2 then is the module not compatible with a LOGO! 0BA5. Read also this Siemens FAQ: Compatibility overview of LOGO! Basic and LOGO! Expansion modules. |
| 7/4/2025 2:01 PM | |
|
Joined: 7/4/2025 Last visit: 8/6/2025 Posts: 3 Rating:
|
IT'S AN AM2 RTD-OBA1 MODULE. IT SHOULD BE COMPATIBLE WITH THE OBA5 CPU |
| 7/4/2025 3:40 PM | |
|
Joined: 12/18/2014 Last visit: 1/2/2026 Posts: 36394 Rating:
|
If the RUN/STOP LED on the AM2 RTD is constantly lit, the expansion module is not communicating with the base module. Is the slider on the expansion module moved all the way to the left? AttachmentLOGO! Soft Handbuch 0BA5 05_2006 englisch pages 34+35.pdf (525 Downloads) |
This contribution was helpful to
|
|
| 7/5/2025 3:10 AM | |
|
Joined: 12/18/2014 Last visit: 1/2/2026 Posts: 36394 Rating:
|
I'm glad it's working now. The main thing is, that it's working now. |
Follow us on