(0)| 7/22/2025 8:50 AM | |
|
Joined: 8/3/2009 Last visit: 1/16/2026 Posts: 16644 Rating:
|
Hello Martins_Eng as the screenshot shows... Its a Simatic WinCC V7.3 yes, you can use Taglogging tags in the OnlineTrendControl or OnlineTableControl to show historical data. Also here you can enable the export button and do an export of the shown timespan in the control in Runtime to export as csv the way you ask this question show that you do probably not have very much experience with WinCC V7/8 SCADA systems? I this case try to work with the help system and F1 Key for quickhelp. Also there are some kind of Getting Started: https://support.industry.siemens.com/cs/de/en/view/73505596 Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on