(0)| 5/18/2022 3:20 PM | |
|
Joined: 10/11/2006 Last visit: 1/8/2026 Posts: 6065 Rating:
|
Dear Vivek Kansara, I assume, that MPG is like a pulse train input. With the CPU1200 it is a lot of programming work. The position has to be captured, scaled and sent as position setpoint via SINAPos to the drive, which runs in position controlled mode (basic positioner). When running is setup mode, the drive follows the setpint from the PLC continuous. Therfore the DriveLib helps: https://support.industry.siemens.com/cs/ww/en/view/109475044 Due to the fact, that the position control is done inside the V90 it is smooth and a coparatively dynamic movement. Anyhow, the high end solution is a S7 15xxT with TO external encoder synchronous run.
|
|
With best regards, |
|
| 5/25/2022 11:06 AM | |
|
Posts: 153 Rating:
|
Hello Technology Team, Thanks for the Response. Regards. |
| 7/28/2025 11:49 AM | |
|
Joined: 1/19/2009 Last visit: 1/8/2026 Posts: 8 Rating:
|
Hi vivek I am having the same requirement with same hardware . Can you guide if you have implemented. |
Follow us on