(1)| 7/9/2025 7:21 PM | |
|
Joined: 1/21/2013 Last visit: 1/15/2026 Posts: 4402 Rating:
|
Hi, All right, let's get back to your initial question. The Unified Panels perform internal buffering of trace log messages, but this cannot be controlled or disabled. Tracing itself will slow down the system because it adds extra load. However, I have never seen memory fill up because of tracing. I assume the trace message you're complaining about doesn't explain your problem. It's just an additional result of the main problem you're experiencing. Further investigation is probably necessary to solve your problem. This would require you to provide additional information. However, it would be best if you provided this information to Technical Support. Kind regards |
This contribution was helpful to
|
|
Follow us on