(3)| 3/25/2013 4:10 PM | |
|
Joined: 9/23/2005 Last visit: 1/9/2026 Posts: 4443 Rating:
|
Hi, The manual “SIMATIC SIMATIC S7-1500, ET 200MP, ET 200SP System diagnostics” (http://support.automation.siemens.com/WW/view/en/59192926) gives a good overview of how to get diagnose of the S7-1500. I posted some general considerations about diagnose at https://www.automation.siemens.com/BR/tf/WW/en/Posts/89419#top I post here a sample project that shows how to use the instruction LED to get some diagnose data in the user program. The sample program is located in the Block_1 (FB1) called from Main_1 (OB1) and using the instance data block “aaa” (DB1), where the relevant data are allocates. In Block_1 I call the block LED several times, to get different types of information.The Watch table shows also the relevant data for the user. Note: not all functions could be 100% simulated in PLC Sim AttachmentDIAG_LED.zip (2421 Downloads) |
Last edited by: O_Moderator at: 6/25/2013 8:24 AMDenilson Pegaia |
|
This contribution was helpful to
|
|
| 11/13/2018 1:22 AM | |
|
Joined: 10/13/2017 Last visit: 4/8/2025 Posts: 4 Rating:
|
Would you be able to provide this example (attachment) in a newer format of TIA Portal than that of v12? Ideally v13 at minimum, or preferably v15. |
Last edited by: dlevine at: 11/13/2018 1:24:13 AM |
|
| 9/24/2020 1:14 PM | |
|
Posts: 96 Rating:
|
DEAR SIR, CAN I GET THE DIAG_LED PROGRAM IN HIGHER VERSION AS ,I AM USING TIA PORTAL V15.1 UPDATE 4. THANKS & REGARDS, SAMIR |
| 8/7/2025 2:10 PM | |
|
Joined: 1/8/2024 Last visit: 12/10/2025 Posts: 1 Rating:
|
I have cpu 1214c dc/dc/dc in tia v17 ,it is possible to doing that ???? |
Follow us on