(0)| 8/22/2025 6:48 AM | |
|
Joined: 8/3/2009 Last visit: 1/9/2026 Posts: 16629 Rating:
|
Hello AutoGen_6546909 This sounds strange... The behaviour is of course not usual I would recommend doing a Reset to factory settings with Prosave and then transfer the project again to the panel. Use the latest Update in TIA for your Version and use the latest available Image Update for the Panel. https://support.industry.siemens.com/cs/ww/en/view/19701610 (I would also recommend doing a full backup of the Panel before reseting it, that you can switch back in case of a problem or issue; but do not only restore after the reset of the panel, a fresh reload of the project would be the best way) Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on