(0)| 8/18/2025 3:42 PM | |
|
Joined: 10/12/2015 Last visit: 10/23/2025 Posts: 19 Rating:
|
Hi I am having a issue with one of our lines today, we have a old line that was running in TIA17. We use dynamic values in multiple alarms. On the TIA17 line it was working fine, on the new line we are using TIA19, with the same comfort HMI but with a new s7-1514SP-2. The issue I am having is that as soon as multiple alarms are triggered that use dynamic values the HMI disconnects from the PLC with a 2700000 system alarm. I am trying to trigger let us say 8 alarms that pull in a dynamic string field for each one that has a length of 8. We have also then Updated the old PLC to V19 and that one still runs fine, with the only difference now between the 2 systems being the one that works runs on a 1512SP F-1 and the one that does not work is a 1514SP-2 which is non safe. Anyone run into this issue before? Regards ------------------------------------------------------------------------------------------ |
Last edited by: MorneF at: 08/18/2025 17:30:34Last edited by: Moderator_Lan at: 08/19/2025 04:52:53New subject after splitting |
|
| 8/29/2025 3:11 PM | |
|
Joined: 10/12/2015 Last visit: 10/23/2025 Posts: 19 Rating:
|
Hi Murof I made one thank you. Regards Morne |
Follow us on