(0)| 8/20/2025 9:17 AM | |
|
Joined: 4/18/2025 Last visit: 9/25/2025 Posts: 5 Rating:
|
Good morning, I try to communicate to a router by sending http request. For this I use the FB LHTTP_PostPut from Siemens. I try 2 different actions : api/login and api/messages/actions/send. At the first attempt for 1 http request, it works, I receive a response code of 200 in the LHTTP_PostPut (that means the request was processed successfully), and the output done is true. The message from the router is store in a array “reponseData”. I receive this first message correctly. After when I send a second http request the Fb LHTTP_PostPut returns me an error 8641 with subfunction 8383. 16#8383 The value at the SRC_INDEX is outside the high limit of the ARRAY. The strange thing is I still receive the response code of 200, but the message from the router can not reach my Siemens PLC. Each time I turn off and turn on the Siemens PLC, the first request is working but the following ones, no. For the request api/messages/actions/send, the router sends a SMS. Even If I dont receive a message from the LHTTP_PostPut, the SMS is sent by the router, for the second request and more . I tried to find the solution on the forum, youtube, chatGPT, but no "solution" is working. I changed the parameter of the LHTTP_PostPut , put the keepConnection to False and to True, I tried to change the user Field (header of the http request): by putting ‘Accept-Encoding: identity$R$LConnection: close$R$L$00’ . But no success until now :( If you have any ideas, it will help me a lot. Thank you in advance for your time. :)
Link for the FB LHTTP_PostPut from : https://support.industry.siemens.com/cs/de/en/view/109780503 Link for the Move_Blk_variant: https://support.industry.siemens.com/cs/de/de/view/109747174/96821112587 |
Last edited by: Moderator_Lan at: 08/20/2025 09:26:07link optimized Last edited by: LeoAG7 at: 09/04/2025 11:21:31Last edited by: LeoAG7 at: 09/04/2025 13:25:44 |
|
Follow us on