(0)| 8/26/2006 1:15 PM | |
|
Posts: 1 Rating:
|
Hello, I have installed Sincom 3.2 in a MMC, and when I try to test itfrom a PC using Scotest.exe the machine always respondsthe sameerror message: -97 (ERR_RESTARTING: RPC return value, if an RPC arrives during restart) I have this problem just in one machine. I have installed Sincom in 3 others identical machines, and I haven't hadany problem. I have tried to remove and reinstalling Sincom in the machine, I have switched off and on the machine... but the responses to any commadsended withScotestare always -97.[:cry:] This is a part of Sincom.log in f:\add_on\ E 08/26/06 10:30:58 32 233 DeleteFile C:\TMP\Trc.shm T 08/26/06 10:31:00 0 235 HostThreadProc pHostData->m_pRPCData NULL M 08/26/06 10:31:00 0 233 Programmstart M8 Release 3.2 T 08/26/06 10:31:00 0 237 pcInitialize() E 08/26/06 10:31:35 -7 233 DdeMTConnection::Poke ( /Plc/DataBlock/Byte[c12,4] ) DdeGetLastError() -> 16393 : NCDDE_LastError() -> 505090a T 08/26/06 10:32:41 0 066 T_MACHINE_M: H8 M8 E 08/26/06 10:33:02 -6 237 DdeMTConnection::Request ( /Plc/DataBlock/Byte[c12,0,19]("!l%d,") ) DdeGetLastError() -> 16393 : NCDDE_LastError() -> 504090a E 08/26/06 10:33:32 -6 237 appendItemToFifo->/Plc/DataBlock/Byte-FAST[c12,1]: ddeData-># E 08/26/06 10:34:02 -7 237 DdeMTConnection::Poke ( /Plc/DataBlock/Byte[c12,0] ) DdeGetLastError() -> 16393 : NCDDE_LastError() -> 505090a T 08/26/06 10:34:12 0 233 CThrProdCtrl::ThreadCancle !!!! E 08/26/06 10:34:32 -6 237 DdeMTConnection::Request ( /Plc/DataBlock/Byte[c12,0,19]("!l%d,") ) DdeGetLastError() -> 16393 : NCDDE_LastError() -> 504090a I have attached 4 files I am using: Sincom.log, sincomerr.log, scvarset.ini, regie.ini. Thanks in advance, Diego AttachmentSincom_files.zip (1194 Downloads) |
Follow us on