9/3/2006 5:56 PM | |
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
Hi Pavel, Normally it is a plug and play card, so you doesn't have to do anything. It is possible that you have to remove some unused cards so that the routine can find the CP5512 as new. Please also consider with which versions of windows the CP5512 is working together. AttachmentNET_PC_CP_OS_e.pdf (910 Downloads) |
Last edited by: Late at: 9/3/2006 5:58 PMI hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
9/4/2006 12:11 PM | |
Posts: 4 Rating:
|
Hello Wizard I've made mistake. I thought SP4 and wrote SP5. I am running the card under Win2000 SP4. |
9/4/2006 2:03 PM | |
Posts: 4 Rating:
|
My notebook supports 32-bit PC-Card. There should be no problem. |
Follow us on