9/19/2006 11:50 AM | |
Posts: 7 Rating:
|
Hello, I've got a CP342-5 which must communicate with 2 ET200M with IM153-1 in each. My CP342-5 is a master DP. When i use the DP_RECV bloc in th OB1, I've got the status 8090 which means an incorrect address but my address is good. No DP_Send is used because I only have AI card in the ET200M. Help please AttachmentSIEMENS_ALARMES V2.1.zip (929 Downloads) |
9/19/2006 12:54 PM | |
Posts: 7 Rating:
|
Oh yes! I'm stupid! Thanks a lot.[:blush:] |
Follow us on