7/9/2010 8:10 PM | |
Posts: 13 Rating:
|
Hello dear LOGO! experts , I have encountered with three problems and i hope that you can help me to solve them. 1. Is it possible in programming of LOGO to make an on-delay according to cycle time instead of mili seconds? for example i want to have an on-delay with period defined as 3 cycle times. [schnippschnapp]
Other two questions are splittet into the following threads need to see and register the start time . i want to monitor and archive the status of digital . |
Last edited by: O_Moderator at: 7/12/2010 12:09 PM |
|
7/12/2010 12:36 AM | |
Joined: 3/4/2009 Last visit: 10/28/2020 Posts: 57 Rating:
|
Hi Ayoob.M 1) Have a look at the attached program. AttachmentOn delay according to program cycles.zip (564 Downloads) |
This contribution was helpful to
1 thankful Users |
7/13/2010 5:42 PM | |
Posts: 13 Rating:
|
Hi dear miltos, i downloaded your file, it works and has solved my problem, thankyou so much. |
7/13/2010 9:55 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating:
|
Hi Ayoob.M, look at the attachment and find an optimized circuit... Best regards Betel _________________________________________________ Perhaps helpful links: AttachmentOn delay according to program cycles (optimation).zip (570 Downloads) |
==> Meine TAG-Listen: "deut." |
|
This contribution was helpful to
1 thankful Users |
7/14/2010 1:52 PM | |
Posts: 13 Rating:
|
Hi Betel, thanks a lot, the circuit is simplified well. best regards... |
Follow us on