(0)| 9/9/2010 5:52 PM | |
|
Posts: 134 Rating:
|
what is the color of your card ? |
| 9/10/2010 8:15 AM | |
|
Posts: 719 Rating:
|
Hello mike 123a, your light brown Module can be written by LOGO! 0BA4 and 0BA5, the Model 0BA6 only can read it. If you want write to Card with 0BA6 you must use the violet or dark brown (with Backup Battery) Card. See this Data Sheet: http://support.automation.siemens.com/WW/view/en/17907754 The Memory Card will be replace the internal Memory of the LOGO! and is used only at runtime, will say, when the Card is unplugged, the Program is on Card and not in LOGO! For copy protect use a password in your .lsc then the Card (if the PW is unknown) only can used or erased by a LOGO! with Display. I hope this helps. Best regards ring24h |
Last edited by: ring24h at: 9/10/2010 8:19 AM |
|
Follow us on