(0)| 11/8/2010 2:42 PM | |
|
Joined: 1/4/2007 Last visit: 12/16/2025 Posts: 1197 Rating:
|
Hello OveBDK, Can you publish the data sheet into this forum, so that I can tke a look into it? Best regards Siwarexi |
| 11/8/2010 7:47 PM | |
|
Posts: 9 Rating:
|
Hello expert. There's a specification in attached PDF file. Main items: Electrical Characteristics Configuration: Four active arm bonded Wheatstone bridge strain gage Zero balance: ±10% full scale Bridge resistance: Input: 345 Ohms minimum; Output: 350 Ohms typical Excitation: 10 Vdc recommended, 12 Vdc maximum Full scale output: 3.33 mV/V ±2% Attachmentmrt460___multi_range_pressure_transducer.pdf (308 Downloads) |
Follow us on