(0)| 1/25/2011 8:17 AM | |
|
Posts: 8 Rating:
|
Hi All! I'm working Simoreg connect PLC S7_400 via Profibus. This is a hardware configuration. ( file attachment). Memory area in Simoreg, there are 6 word Input ( 150...161) and 6 word output ( 150...161). When i read the PLC program. i see, they are use IW152 in Simoreg to control speed ( setpoint). (PLC sends the value to the IW152 Simoreg to set the speed). So, the memory input ( IW150, 154, 156, 158, 160) and memory output in Simoreg ( QW152, 154,156,158,160) What function? memory cells used to reset any error in Simoreg? i have read the manual Simoreg.Simoreg have memory cells that control and status display.( Control Word 1, control word 2, status word 1 , status word 2 ...). To use the PLC to take control parameters and Simoreg. the WORD is this? need to set any parameters? Please tell me! Thanks you so much! Splitted from How to setpoint speed to SIMOREG DC-MASTER (6RA70) via profibus. |
Last edited by: O_Moderator at: 1/25/2011 10:52 AMnew subject after splitting |
|
| 1/26/2011 7:38 AM | |
|
Posts: 8 Rating:
|
Thanks for KSN! |
Follow us on