8/18/2011 2:06 PM | |
Posts: 10 Rating:
|
Dear Experts, We have a network of two S7-416 2DP, and for "Online Access" we use Ethernet. We have Sinamics control units in both the PLC, on their own profibus network. 1st PLC IP 192.168.1.25 2nd PLC IP 192.168.1.35 The Sinamics of first PLC, on which a CP443-Advanced is connected, is accessible. The Sinamics of second PLC, on which a CP443-Basic is connected, is not accessible. I have tried Online access window in Scout to the correct IP address and wrong IP I tried Online access point in commissioning interface to standalone access AND S7ONLINE, both. Still not accessible. Please help. Warm Regards, Kiru...! AttachmentSinamics.zip (343 Downloads) |
Follow us on