(0)| 10/10/2011 7:32 AM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hello, Yes, I think is possible to make it with LOGO!. You will need a functional descriptions of the machine plus electrical drawings in order to build the same. Take a look at Where can you find examples of application or program examples for LOGO! ? These examples could helps you in some points. Basically there is needing to prepare logic for: 1. Start/Stop rotating depending of emergency stop, manual start/stop, eventually counts of turns... 2. Start/Stop lifting/lowering of the machine with almost the same conditions including Auto Mode, which is depend from the height of the package. Best regards, Hristo MIhalev |
Follow us on