(0)| 12/5/2011 7:56 PM | |
|
Joined: 4/29/2010 Last visit: 12/16/2025 Posts: 2 Rating:
|
Hi, Mata, I have exactly the same problem. In my old and new computer (Both are Win XP), I have Simatic Step 7 v5.5.1.0 and Scout v4.1.5.6 installed. The scout in my old computer can create and edit DCC; the scout in my new computer cannot create or edit DCC. If I retrieve a zipped project which has DCC program from my old computer, it changed the DCC object name and opened with a question mark. I cannot edit it. Is it possible the problem related to CPU. I would be shocked if it is true. But logically, it is possible. My old computer is four years old from dell (D630 with 2G memery, Intel Core 2 Duo CPU); my new computer isHP I got two month ago (HP EliteBook 8560w with 4G memery, intel core i7 CPU). How about your case? Thanks Gary Attachmentsoftware_version_compare.zip (621 Downloads) |
Follow us on