(0)| 2/6/2012 5:15 AM | |
|
Posts: 36 Rating:
|
Sir, i am facing problem about TIA V 11 software. I am using S7 !200 CPU 1214 AC/DC/Rely. I am download the program in the cpu. but when i off he power and after 5 to 10 min on the power the cpu goes in to the stop made. i saw the onnline dignostics then the error shows that the internal memory currupt. I did factory reset of the CPU and download the program. After power off i am facing same problem. CPU goes in to stop mode. i attach the picture about the error. Please do reply fast... AttachmentE1.zip (361 Downloads) |
Last edited by: O_Moderator at: 2/7/2012 10:27 AMnew subject after splitting from /tf/WW/en/Posts/68933#top |
|
| 2/6/2012 6:39 AM | |
|
Joined: 8/31/2010 Last visit: 12/6/2025 Posts: 1525 Rating:
|
What is the FirmWare version of the CPU you are using? Are you using PID controller in your S7-1200? Possible Solution: 1. Ensure you use the FW v2.2.0 (you can download from here - Operating system updates for CPU 1214C, COMPACT CPU, AC/DC/Relay) for which you also need atlesast STEP 7 Basic v11 SP2 in turn. 2. Perfrom a "reset to factory settings" option and 3. Also always download the program changes using the "Software (all blocks)" in your controller. This ensures that all the blocks are downloaded into the controller and prevents inconsistencies (even after a power failure). This should probablly fix the issue. Check and get back on this. |
|
Like it? Rate it! |
|
Follow us on