3/14/2007 12:02 PM | |
Joined: 10/11/2006 Last visit: 8/29/2025 Posts: 6037 Rating:
|
Hello, yes it is possible to make a synchronism application between two Masterdrives MCs via Profibus with peer to peer communication. Of course it is essential for a good synchronism that the DP cycle time should not be too high (3,2 ms or lower is recommended). Attached a basic application and a manual. Regards, TechTeam Attachment4_synchronism_(autark_via_profibus).zip (701 Downloads) |
With best regards, |
|
Follow us on