(0)| 5/24/2012 8:40 AM | |
|
Posts: 129 Rating:
|
i want to change a different velocity upto reached distance(200mm)....i did a sample program for that operation using a MC_MOVERELATIVE Block to change the velocity of the motor.....but iam facing problem is in forward direction maintaining a as per given velocity but inreverse direction it maintaining a constant velocity (high or low) upto the reached distance....what is the problem....what i'll do for maintaning a variable velocity for forward & reverse movement...thanks ur help???????? can we change the velocity randomly......possible or not????plz help me sir... AttachmentHSC.zip (906 Downloads) |
Last edited by: peter jenny at: 5/24/2012 1:05 PMplz give the reply sir |
|
| 5/24/2012 8:53 AM | |
|
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
Thread closed, because question is already published in the following thread MC_MOVERELATIVE in s7-1200 plc. Best regards O_Moderator |
This contribution was helpful to
|
|
Follow us on