(0)| 3/30/2007 6:36 PM | |
|
Joined: 3/26/2007 Last visit: 1/15/2026 Posts: 7 Rating:
|
Hi all!!!!!!!!!!!!!!!! Ihavebeen trying to communicate these devices with Modbusprotocol, the Drive isa VLT2800 and PLC 224. The param. in the diriveis ok (parity, velocity..., i attachmentthemanual in pdf) Here an ExampleAll value in hexadecimal EXAMPLE 1: Start Motor, Run Speed 40% Modbus function 0FHEX (Force Multiple Coils). Message sent to Modbus RTU from Modbus master Byte 0 Byte 1 Byte 2 Byte 3 7C 04 99 19 Modbus message string: [01] [0F] [00] [00] [00] [20] [04] [7C] [04] [99] [19] [37] [43] [7C]+[04]: Start Command: 0000010001111100 = 047CHEX(reversed) Modbus message string: [01] [0F] [00] [00] [00] [20] [04] [7C] [04] [99] [19] [37] [43] [99]+[19]: NOTE: Speed Command: 4000HEX = 100% speed 40% of 4000HEX = 1999HEX(reversed)
Attachmentmodbus_rtu_vlt__serie_2800.pdf (732 Downloads) |
Follow us on