11/9/2012 6:40 AM | |
Joined: 12/4/2007 Last visit: 7/25/2025 Posts: 7 Rating:
|
Dears, I make a configuration with 828D baisc +S120 for a turning machine tool, and use 1PH8165-1DB00-0BA1 as main spindle motor, but some data shows in our documents need your help to clarify. 1. as power limited in SLM, for 13KW in SLM, so I choose ALM as power module, to use the motor as 16KW. 2. as 1PH81651DB000BA1.pdf shows, there is N max inv, what's this data means, does it means if the motor's speed above Nmax inv, do we need a VPM between the 1PH8165-1DB00-0BA1 and 6SL3120-1TE24-5AA3? or we can only operate the motor 1PH8165-1DB00-0BA1 under N max inv if we use ALM module. thanks. AttachmentD:\tmp\download\Desktop_configuration all.pdf (510 Downloads) |
Last edited by: CS Moderator at: 11/9/2012 2:22 PMDocument reattached |
|
Follow us on