10/18/2013 11:11 AM | |
Posts: 32 Rating:
|
Hello Deputy, thank you very much for your elaborate description of selecting the cable for servo motor of specified type. But i think i did a mistake in typing of the cable type. It is- servo motors of type no.- 1FT6062-6AC71-3FB1. motion connect cable of type no.- 6FX8002-5DG01-2GA10. So according to your description cable is suitable for the above motor. But The problem is- at the motor end, i am unable to connect this cable connector with the motor flange socket.In my opinion the male connector of the cable is not maching with the female coonector socket of the motor. Could you please check the photographs and suggest your opinion if these two are compatible or not. With regards, Anirban Mandal Siemens Ltd.
Attachmentservo.zip (464 Downloads) |
Follow us on