12/6/2013 10:19 AM | |
Joined: 11/23/2011 Last visit: 9/9/2025 Posts: 202 Rating:
|
Hello Sven Peter, I would also like to help you with some information. You can have a look on this quite new application examples for home automation with communication for more than one LOGO! modules through Ethernet. http://support.automation.siemens.com/WW/view/en/64143308 http://support.automation.siemens.com/WW/view/en/68585344 http://support.automation.siemens.com/WW/view/en/68585346 Reading the examples you can choose which communication, Master-Slave or Server-Client, is more suitable for your case. You can also use both communications in one application like in this examples. (All the three examples can be linked together) Thereare also completed codes and step-to-stepdocumentations for download. Greetings, KM_AS |
This contribution was helpful to
1 thankful Users |
12/6/2013 3:25 PM | |
Joined: 11/23/2011 Last visit: 9/9/2025 Posts: 202 Rating:
|
Hello SvenPeter, |
Follow us on